Which Switch: Who Cares if it’s AC or DC?! Rudy Ramos
Have you ever tried to use a switch in an application and wondered whether the difference between the AC and DC rating on switches really matters? ­­There is a fallacy that any switch can be used so long as its current rating exceeds the maximum load requirements in the circuit. Who cares if it’s AC or DC, it’s only a 12VDC system right? Wrong; when it comes to switches, the differences in current-carrying capacity are dramatically different between AC and DC circuits and this is typically reflected in the switch’s AC and DC ratings.

All Authors

Show More Show More
View Blogs by Date