New Tech Tuesdays: Reliable Internet Access Anywhere, Anytime with TE Connectivity's LEMBAS LTE/GNSS USB Modem Rudy Ramos
Portable USB modems are a convenient and versatile solution for providing internet connectivity to devices that do not have built-in cellular connectivity or lack reliable Wi-Fi® access.

New Tech Tuesdays: SIM Cards and LTE-Enabled Module Provide Cellular Solutions Tommy Cummings
Let's evaluate three products that are crucial to machine-to-machine and Internet of Things project development.

Asset Tracking with Nordic and Medium One Greg Toth
The Nordic nRF9160 Development Kit (DK) together with the cloud-based Medium One IoT Prototyping Sandbox provides hardware, software, and cloud-based tools to create LTE-connected GPS asset tracking and IoT applications.

Use the Renesas AE-CLOUD2 to Send GPS Data to the Google Cloud IoT Greg Toth
Use this kit to prototype sensor and location tracking applications that connect to the Google Cloud IoT via Ethernet, Wi-Fi, or LTE Cat-M1/Cat-NM1/EGPRS LTE cellular networks. Create applications that read sensors, connect to the Internet, and communicate real-time sensor data to the Google Cloud.

Wireless in 2014: The Industry at Mid-Year Barry Manz
As members of the RF and microwave industry make their annual pilgrimage to IMS 2014 (this year in Tampa), I offer my opinion on the industry’s overall health at mid-year. Fortunately, it appears that it’s going to be hot in Tampa in more ways than one. Just how hot depends on many factors, many of them company-specific, so there’s no single answer to “How’s business?” Nevertheless, a realistic approach with this blog is to look at key markets in the wireless industry.

5G: Coming Sooner than Later Barry Manz
Now that most of us have smartphones with LTE capability, life is good. Video streams nicely, downloads are quick, and if you happen to be standing next to a base station data rates can be truly impressive. It won’t be long before LTE Advanced shoves LTE aside with data rates 10 times faster, which means we will be able to download HD movies very quickly and do virtually anything else almost instantly. That however, is apparently not enough for the wireless industry, if developments in South Korea and the European Union are any indication.

All Authors

Show More Show More
View Blogs by Date