Now at Mouser: Power Integrations InnoSwitch3-AQ Flyback Switcher IC for Electric Vehicles

New Product Announcement

Connect With Us


Now at Mouser: Power Integrations InnoSwitch3-AQ Flyback Switcher IC for Electric Vehicles

December 2, 2020 - Mouser Electronics, Inc., the industry's leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components, is now stocking the InnoSwitch™3-AQ flyback switcher IC from Power Integrations.

The InnoSwitch3-AQ flyback switcher IC integrates a 750V MOSFET with Fluxlink™ feedback for automotive applications. The IC combines primary and secondary controllers and safety-rated feedback into a single IC. This combination offers output voltage regulation even with a wide 30VDC to 550VDC input voltage range. The InnoSwitch3-AQ IC provides up to 90% efficiency across the full load range and is AEC-Q100 qualified.

The IC offers protection features such as line over- and under-voltage protection, output over-voltage and over-current limiting, and over-temperature shutdown for automotive applications. The InnoSwitch3-AQ IC is ideal for automotive applications such as traction inverters, DC-DC converters, and on-board chargers.

For more information, visit https://www.mouser.com/new/power-integrations/power-integrations-innoswitch3-aq-ic/.

As a global authorised distributor, Mouser offers the world's widest selection of the newest semiconductors and electronic components — in stock and ready to ship. Mouser's customers can expect 100% certified, genuine products that are fully traceable from each of its manufacturer partners. To help speed up the design process for customers, Mouser's website hosts an extensive library of technical resources, including a Technical Resource Centre, along with product data sheets, supplier-specific reference designs, application notes, technical design information, engineering tools and other helpful information.

About Mouser

2026 - Mouser Electronics is an authorized semiconductor and electronic component distributor focused on New Product Introductions from its leading manufacturer partners. Serving the global electronic design engineer and buyer community, the global distributor's website, mouser.com, is available in multiple languages and currencies and features more than 6.8 million products from over 1,200 manufacturer brands. Mouser offers 28 support locations worldwide to provide best-in-class customer service in local language, currency and time zone. The distributor ships to over 650,000 customers in 223 countries/territories from its 93,000m², state-of-the-art distribution facilities in the Dallas, Texas, metro area. For more information, visit https://www.mouser.com.

About Power Integrations

2026 - Power Integrations, Inc., is a Silicon Valley-based supplier of high-performance components used in high-voltage power conversion. Power Integrations' integrated circuits enable compact, energy-efficient AC-DC power supplies for a vast range of electronic products. These include smartphones, appliances, smart utility meters, LED lights, and numerous industrial applications. Power Integrations SCALE gate drivers are critical components in high-power systems, such as solar and wind energy, industrial motor drives, electric vehicles, and high-voltage DC transmission lines. Since its introduction in 1998, Power Integrations' EcoSmart energy-efficiency technology has prevented billions of dollars of energy waste and millions of tons of carbon emissions. Reflecting the environmental benefits of its products, Power Integrations' stock is a component of clean-technology stock indices sponsored by Cleantech Group LLC and Clean Edge.

Trademarks

Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.

For further information, contact:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833
For press enquiries, contact:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764