Noise in ADC Signal Chains
Understanding How Amplifier Noise Contributes to Total Noise in ADC Signal Chains
By Umesh Jayamohan, Analog Devices
Featured Products
Resources
Introduction
Analog-to-digital converters (ADCs) provide optimal performance when the analog inputs are driven to their rated
full-scale input voltage, but in many applications, the maximum available signal differs from the specified
voltage and may need to be adjusted. A useful device for handling this requirement is a variable-gain amplifier
(VGA). Understanding how the VGA affects the ADC's performance will help in optimizing performance of the entire
signal chain.
This article analyzes noise in a circuit that uses the AD9268 dual 16-bit, 125-/105-/80-MSPS, pipelined ADC, and
the AD8375 ultralow distortion IF VGA. The signal chain includes a VGA—used at a gain setting of +6 dB, a
5th-order Butterworth low-pass filter with a –3-dB roll-off at 100 MHz, and the ADC. Noise calculations will be
shown for the amplifier and filter, as they dictate the dynamic performance of the ADC over the band of
interest.
Problem
Many real-world applications using high-speed ADCs need some sort of driver, amplifier, or gain block that scales
the input signal to the full-scale analog input range1 to ensure optimum signal-to-noise ratio (SNR) and
spurious-free dynamic range (SFDR). In addition, a differential amplifier could also convert a single-ended
signal to a differential signal to drive the ADC. Being active, these components contribute noise at the ADC
front end. The integration of this noise over the operational bandwidth will degrade the conversion performance.
The choice of an appropriate ADC for an application depends on many factors, including:
- Analog input range
- Input frequency/bandwidth
- Desired resolution/SNR
- Desired SFDR
Some applications require both high dynamic range and high resolution. The AD9268 is very good choice for
these applications, delivering 78.2-dBFS (dB relative to full-scale) SNR and 88-dBc SFDR at a 70-MHz
intermediate frequency.
At the system level, the ADC front-end could use an amplifier, a transformer, or a balun, but implementations
using an amplifier are most common. An amplifier could be used for one or more of the following reasons:
- Provide gain to the input signal to increase the ADC resolution.
- Buffer or transform the impedance between the input source and the ADC.
- Convert a single-ended input signal to a differential output signal.
The AD8375 VGA, which maintains high linearity and uniform noise performance over its various gain settings,
can be used to convert single-ended signals to differential. These characteristics make it a good candidate
for driving the ADC at higher intermediate frequencies. Unfortunately, the presence of an active device—the
amplifier—in the signal chain can limit the ADC's performance.
Example
Figure 1 shows the circuit topology used in performing the noise calculations. The AD8375 has a
high-impedance differential output (16 kω||0.8 pF). A 5th-order low-pass antialiasing filter (AAF) with
100-MHz bandwidth and 150-ω input and output impedances interfaces the amplifier to the ADC. The frequency
response of the circuit shown in Figure 1 can be seen in Figure 2.
Figure 1: The AD8375, AAF, and
AD9268 signal chain.
Figure 2:
Frequency response of the AD8375, AAF, and AD9268 signal chain.
Performance
System designers may not expect the amplifier driving the ADC inputs to degrade the overall dynamic
performance of the system, but the fact that a driver and ADC combo was chosen for one application does not
mean that it will provide the same great performance in another application. The technique described here
allows a systems engineer to estimate the expected performance before choosing an amplifier.
Figure 3 shows two different setups: Figure 3(a), which uses passive coupling to the converter, is available
as the default option on the customer evaluation board. The passive front-end network uses a transformer or
balun to convert the single-ended signal to differential, along with a passive low-pass filter that rolls
off at about 200 MHz. Figure 3(b) shows the optional amplifier path. A comparison of the noise contributed
by these two setups follows. A single-tone fast Fourier transform (FFT) at a low intermediate frequency (10
MHz) is used to calculate the noise added by the amplifier.
Figure 3: Typical ADC
front-ends: (a) passive. (b) active.
Two techniques are typically used for analyzing the noise, but each can be cumbersome. Noise spectral density
(NSD) defines the noise power per unit bandwidth. It is represented in mean-square dBm/Hz or dBFS/Hz for
ADCs and rms nV/√Hz for amplifiers. This incompatibility in units provides an obstacle to calculating system
noise when an amplifier is driving an ADC.
Noise figure (NF) is the log ratio of input SNR to the output SNR expressed in decibels. This specification,
commonly used by RF engineers, makes sense in a purely RF world, but attempting to use NF calculations in a
signal chain with an ADC can lead to misleading results.2
An alternate, but more effective, technique is to "de-normalize" the noise density, representing it as an rms
noise voltage rather than a mean-square voltage. This method, as described here, is straightforward and
allows a clear analysis of the system noise.
Figure 4 and Figure 5 show the low-frequency single-tone FFTs of the two front ends. Note that the passive
front end has 77.7-dBFS SNR, while the active front end has 72.5-dBFS SNR, 5.2 dBFS lower than the ADC's
expected performance.
Figure 4: FFT
of a 10-MHz analog input tone for the circuit of Figure 3a.
Figure 5: FFT
of a 10-MHz analog input tone for the circuit of Figure 3b.
Umesh Jayamohan is an applications
engineer in the High Speed Converter Group at Analog Devices in Greensboro, NC. Umesh received a BSEE from
University of Kerala, India in 1998 and a MSEE from Arizona State University in 2002, and has over seven
years of experience as a design and applications engineer.