Analog Devices AD-GMSL2ETH-SL Edge Compute Platform, Now Available at Mouser, Supports Machine Vision in Autonomous Robots and Vehicles

New Product Announcement

Connect With Us


January 29, 2025Mouser Electronics, Inc., the industry’s leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components™, is now stocking the AD-GMSL2ETH-SL edge compute platform from Analog Devices, Inc. (ADI). The advanced single-board computer (SBC) enables low-latency data transfer from eight Gigabit Multimedia Serial LinkTM (GMSL) interfaces to a 10Gb Ethernet link. The AD-GMSL2ETH-SL is designed for machine vision and real-time sensor fusion in applications, including autonomous robots and vehicles. 

The ADI AD-GMSL2ETH-SL, now available at Mouser, features two MAX96724 Quad Tunneling GMSL2/1 to CSI-2 deserializers, enabling connectivity with eight GMSL cameras. Each camera supports up to 6 Gbps per channel. Video data is transferred from the MAX96724 deserializers to an AMD KV26 System on Module (SOM) via MIPI CSI2 interfaces. The SOM aggregates video data from all eight GMSL cameras into a 10Gb Ethernet link, ready to be sent to a central processing unit.

The AD-GMSL2ETH-SL supports IEEE 1588 Precision Time Protocol (PTP) with hardware timestamping for accurate synchronization with host systems and other edge devices, while a web-based user interface is available for system configuration and control. This user interface allows users to adjust parameters for camera control and trigger PTP synchronization, general-purpose I/O (GPIO) configuration, and visualize system diagnostics. The edge compute platform also features an embedded graphic user interface (GUI) for easy integration, an ideal feature for complex systems such as robotics. The platform is accompanied by an open-source software stack, FPGA design, and reference applications, allowing designers to quickly begin software development based on a proven implementation. The AD-GMSL2ETH-SL edge compute platform is ROS2 compliant.  

To learn more, visit https://www.mouser.com/new/analog-devices/adi-ad-gmsl2eth-sl-edge-compute-platform/.

 

As a global authorised distributor, Mouser offers the world's widest selection of the newest semiconductors and electronic components — in stock and ready to ship. Mouser's customers can expect 100% certified, genuine products that are fully traceable from each of its manufacturer partners. To help speed up the design process for customers, Mouser's website hosts an extensive library of technical resources, including a Technical Resource Centre, along with product data sheets, supplier-specific reference designs, application notes, technical design information, engineering tools and other helpful information.

About Mouser

2026 - Mouser Electronics is an authorized semiconductor and electronic component distributor focused on New Product Introductions from its leading manufacturer partners. Serving the global electronic design engineer and buyer community, the global distributor's website, mouser.com, is available in multiple languages and currencies and features more than 6.8 million products from over 1,200 manufacturer brands. Mouser offers 28 support locations worldwide to provide best-in-class customer service in local language, currency and time zone. The distributor ships to over 650,000 customers in 223 countries/territories from its 93,000m², state-of-the-art distribution facilities in the Dallas, Texas, metro area. For more information, visit https://www.mouser.com.

Trademarks

Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.

For further information, contact:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833
For press enquiries, contact:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764