New at Mouser: ams OSRAM AS7050 Medical and Health Sensors for Smart Devices and Wearables

New Product Announcement

Connect With Us


June 15, 2022Mouser Electronics, Inc., the industry’s leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components™, is now shipping the AS7050 medical and health sensor from ams OSRAM. The AS7050 provides design engineers with next generation biosignal conversion for a variety of applications, including smart devices; heart rate, electrocardiogram (ECG) and photoplethysmography (PPG) monitoring; optical sensor platforms; wearables and more.

The ams OSRAM AS7050, available from Mouser Electronics, is a biosignal sensor analog front end that offers up to eight LED driver outputs, samples up to six photodiode inputs, and includes support for external electrodes, enabling the highest flexibility for multiple LED and photodiode arrangements in different applications. The analog front end provides two analog-to-digital converter (ADC) channels for simultaneous PPG and ECG measurements and an automatic photodiode offset control. The AS7050 sensor operates from a supply voltage range of 1.7 V to 1.98 V and features a 1 MHz fast-mode plus, 400 kHz fast mode, and 100 kHz standard mode through an I²C bus for maximum efficiency.

Mouser also stocks the ams OSRAM Evaluation Kit for the AS7050, which includes a main board and breakout board for full flexibility. The breakout board incorporates a biosensor, temperature sensor, accelerometer, and electrodes that can be reconnected to the main board via flexible printed circuit (FPC) cable or external electrodes. The breakout board can also be connected to a wristband via a Molex PicoBlade connector.

To learn more about the ams OSRAM AS7050 sensor, visit https://www.mouser.com/new/ams-osram/ams-osram-as7050-medical-sensor/.

 

As a global authorised distributor, Mouser offers the world's widest selection of the newest semiconductors and electronic components — in stock and ready to ship. Mouser's customers can expect 100% certified, genuine products that are fully traceable from each of its manufacturer partners. To help speed up the design process for customers, Mouser's website hosts an extensive library of technical resources, including a Technical Resource Centre, along with product data sheets, supplier-specific reference designs, application notes, technical design information, engineering tools and other helpful information.

About Mouser

2026 - Mouser Electronics is an authorized semiconductor and electronic component distributor focused on New Product Introductions from its leading manufacturer partners. Serving the global electronic design engineer and buyer community, the global distributor's website, mouser.com, is available in multiple languages and currencies and features more than 6.8 million products from over 1,200 manufacturer brands. Mouser offers 28 support locations worldwide to provide best-in-class customer service in local language, currency and time zone. The distributor ships to over 650,000 customers in 223 countries/territories from its 93,000m², state-of-the-art distribution facilities in the Dallas, Texas, metro area. For more information, visit https://www.mouser.com.

About ams OSRAM

2026 - The ams OSRAM Group is a global leader in optical solutions. By adding intelligence to light and passion to innovation, ams OSRAM enrich people’s lives. This is what they mean by Sensing is Life. With over 110 years of combined history, their core is defined by imagination, deep engineering expertise, and the ability to provide global industrial capacity in sensor and light technologies. They create exciting innovations that enable our customers in the consumer, automotive, healthcare, and industrial sectors to maintain their competitive edge and drive innovation that meaningfully improves the quality of life in terms of health, safety, and convenience, while reducing impact on the environment.

ams is a registered trademark of ams-OSRAM AG. In addition, many of their products and services are registered or filed trademarks of ams OSRAM Group.

Trademarks

Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.

For further information, contact:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833
For press enquiries, contact:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764