Laird Antennas' Trigger Family of Under-Dash Telematics Antennas Now at Mouser

New Product Announcement

Connect With Us


November 29, 2021Mouser Electronics, Inc., the industry’s leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components™, is now stocking the Trigger under-dash antenna family from Laird Antennas. The innovative five-port VPJ and four-port VQJ Trigger devices are IP67-rated, multiport/multiband telematics antennas that offer exceptional cellular 3G/4G/5G/ISM/CBRS, Wi-Fi and GNSS functionality for automotive and Internet of Things (IoT) applications, including transportation, public safety, fleet operations, asset tracking, and in-vehicle and to-vehicle communications.

Laird Antennas VxJ Trigger antennas, available from Mouser Electronics, feature a unique L-shaped format and dual-axis VHB adhesive backing, enabling quick and secure mounting in awkward locations. The antennas can be covertly mounted alongside or over bulky non-metallic objects, such as ventilator ducts, with no drilling required. This allows the devices to be mounted closer to the vehicle's router or gateway, usually located under the dashboard or a seat or in the trunk.

Each Trigger antenna comes with vertical and horizontal V-Pol/H-Pol cellular radiating elements within the same antenna to provide better coverage while offering substantial signal performance improvements and more consistent connectivity and data throughput than traditional antennas. With optimized performance and excellent around-the-vehicle coverage, the Trigger family of devices can be used in either dense urban environments or remote locations where signals may be weak or obstructed.

To learn more, visit https://www.mouser.com/new/laird-connectivity/laird-4-5-port-trigger-under-dash-antennas/.

 

As a global authorised distributor, Mouser offers the world's widest selection of the newest semiconductors and electronic components — in stock and ready to ship. Mouser's customers can expect 100% certified, genuine products that are fully traceable from each of its manufacturer partners. To help speed up the design process for customers, Mouser's website hosts an extensive library of technical resources, including a Technical Resource Centre, along with product data sheets, supplier-specific reference designs, application notes, technical design information, engineering tools and other helpful information.

About Mouser

2026 - Mouser Electronics is an authorized semiconductor and electronic component distributor focused on New Product Introductions from its leading manufacturer partners. Serving the global electronic design engineer and buyer community, the global distributor's website, mouser.com, is available in multiple languages and currencies and features more than 6.8 million products from over 1,200 manufacturer brands. Mouser offers 28 support locations worldwide to provide best-in-class customer service in local language, currency and time zone. The distributor ships to over 650,000 customers in 223 countries/territories from its 93,000m², state-of-the-art distribution facilities in the Dallas, Texas, metro area. For more information, visit https://www.mouser.com.

Trademarks

Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.

For further information, contact:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833
For press enquiries, contact:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764