Mouser Now Stocking UnitedSiC (Now Qorvo) UF4C/SC 1200V Gen 4 SiC FETs for Power Applications

New Product Announcement

Connect With Us


May 25, 2022Mouser Electronics, Inc., the industry’s leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components™, is now stocking the UF4C and UF4SC 1200 V silicon carbide (SiC) FETs from UnitedSiC (now Qorvo®). Part of the extensive line of high-performance SiC FETs, this fourth-generation family of devices offers industry-leading figures of merit in on-resistance, suiting it to power solutions in mainstream 800 V bus architectures in applications such as on-board chargers for EVs, industrial battery chargers, industrial power supplies, DC-DC solar inverters, and more.

The UF4C/SC SiC FETs, available from Mouser Electronics, provide designers with multiple on-resistance and package options. The 1200 V SiC FETs are offered in versions with on-resistance (RDS(on)) values of 23 mΩ to 70 mΩ and either a three-lead TO-247-3L package or a four-lead TO-247-4L package. The TO-247-4L package incorporates a Kelvin gate to deliver ultra-low gate charge and exceptional reverse recovery characteristics, enabling designers to switch inductive loads and any application requiring a standard gate drive.

All the devices in the UF4C/SC family can be safely driven with standard 0 V to 12 V or 15 V gate drive voltage, creating a suitable replacement for silicon IGBTs, FETs, or super-junction devices without changing the gate drive voltage. Other notable features of the UF4C/SC SiC FETs include an exceptional threshold noise margin preserved with a true 5 V threshold voltage, excellent reverse recovery, and a built-in ESD gate protection clamp.

To learn more, visit https://www.mouser.com/new/unitedsic/unitedsic-uf4csc-1200v-gen4-sic-fets/.

 

As a global authorised distributor, Mouser offers the world's widest selection of the newest semiconductors and electronic components — in stock and ready to ship. Mouser's customers can expect 100% certified, genuine products that are fully traceable from each of its manufacturer partners. To help speed up the design process for customers, Mouser's website hosts an extensive library of technical resources, including a Technical Resource Centre, along with product data sheets, supplier-specific reference designs, application notes, technical design information, engineering tools and other helpful information.

About Mouser

2026 - Mouser Electronics is an authorized semiconductor and electronic component distributor focused on New Product Introductions from its leading manufacturer partners. Serving the global electronic design engineer and buyer community, the global distributor's website, mouser.com, is available in multiple languages and currencies and features more than 6.8 million products from over 1,200 manufacturer brands. Mouser offers 28 support locations worldwide to provide best-in-class customer service in local language, currency and time zone. The distributor ships to over 650,000 customers in 223 countries/territories from its 93,000m², state-of-the-art distribution facilities in the Dallas, Texas, metro area. For more information, visit https://www.mouser.com.

Trademarks

Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.

For further information, contact:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833
For press enquiries, contact:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764