Now at Mouser: HARTING’s Standard-Setting T1 Industrial Single Pair Ethernet Products

New Product Announcement

Connect With Us


Now at Mouser: HARTING’s Standard-Setting T1 Industrial Single Pair Ethernet Products

August 20, 2020 - Mouser Electronics, Inc., the authorized global distributor with the newest semiconductors and electronic components, is now stocking T1 Industrial single pair Ethernet (SPE) products from HARTING. Selected by the International Electrotechnical Commission (IEC) as the standardized SPE mating face (IEC 63171-6), HARTING's innovative T1 Industrial products enable transmission of data via Ethernet using just two wires, and also offer simultaneous power supply for terminals using Power over Data Line (PoDL).

HARTING T1 Industrial SPE products, available from Mouser Electronics, allow barrier-free connection of sensors, equipment, and actuator technology into the field level using end-to-end IP-based communications, delivering new space and power efficiencies for a range of industrial and communications applications. The products boast a robust industrial design with locking lever protection, high mating cycles, and 360-degree shielding. In addition to the IEC 63171-6 standardized mating face, these T1 Industrial products also meet cabling standards according to ISO/IEC 11801 and TIA 42.

The new devices support the construction of future-proof SPE communication networks, while also offering remote power supply for all PoDL classes. T1 Industrial SPE products simplify parameter setting, initialization, and programming of communication networks, while simultaneously improving the efficiency of equipment set-up, operation, and maintenance.

To learn more about the T1 Industrial SPE Products, visit https://www.mouser.com/new/harting/harting-t1-industrial/.

As a global authorised distributor, Mouser offers the world's widest selection of the newest semiconductors and electronic components — in stock and ready to ship. Mouser's customers can expect 100% certified, genuine products that are fully traceable from each of its manufacturer partners. To help speed up the design process for customers, Mouser's website hosts an extensive library of technical resources, including a Technical Resource Centre, along with product data sheets, supplier-specific reference designs, application notes, technical design information, engineering tools and other helpful information.

About Mouser

2026 - Mouser Electronics is an authorized semiconductor and electronic component distributor focused on New Product Introductions from its leading manufacturer partners. Serving the global electronic design engineer and buyer community, the global distributor's website, mouser.com, is available in multiple languages and currencies and features more than 6.8 million products from over 1,200 manufacturer brands. Mouser offers 28 support locations worldwide to provide best-in-class customer service in local language, currency and time zone. The distributor ships to over 650,000 customers in 223 countries/territories from its 93,000m², state-of-the-art distribution facilities in the Dallas, Texas, metro area. For more information, visit https://www.mouser.com.

About HARTING

2026 - HARTING is the gold standard in connectivity for industrial environments and mission-critical applications.   As the pioneer in connectivity, HARTING combines the quality and customer service of its family-owned operations with a global footprint backed by in-region manufacturing facilities and local teams with deep engineering expertise.

With a reliable and robust approach to connectivity for any environment, HARTING enables improved efficiency and sustainability and future-proofs the businesses of today to power the innovations of tomorrow.

Trademarks

Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.

For further information, contact:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833
For press enquiries, contact:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764