Superior Sensor Technology’s CP201 Dual Low-Pressure Sensor Now at Mouser
December 16, 2021 - Mouser Electronics, Inc., the industry's leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components, is now stocking the CP201 dual low-pressure sensor from Superior Sensor Technology.
Superior Sensor Technology's CP201 dual low-pressure sensor is a highly integrated sensor with an analog-to-digital converter (ADC), digital signal processor (DSP), and differential and gauge sensors in one module. When this sensor is used for continuous positive airway pressure (CPAP) applications, it employs the NimbleSense™ proprietary architecture that achieves a high dynamic range.
The CP201 offers a 4V maximum voltage rating, 25mA maximum current rating, and -20°C to +85°C operating temperature range. The sensor is designed with a high-reliability plastic enclosure that makes it the ideal combination of high performance and reliability while ensuring a solution optimized for a wide array of ventilation devices.
To learn more, visit https://www.mouser.com/new/superior-sensor/superior-cp201-dual-low-pressure-sensor/.
As a global authorised distributor, Mouser offers the world's widest selection of the newest semiconductors and electronic components — in stock and ready to ship. Mouser's customers can expect 100% certified, genuine products that are fully traceable from each of its manufacturer partners. To help speed up the design process for customers, Mouser's website hosts an extensive library of technical resources, including a Technical Resource Centre, along with product data sheets, supplier-specific reference designs, application notes, technical design information, engineering tools and other helpful information.
2026 - Mouser Electronics is an authorized semiconductor and electronic component distributor focused on New Product Introductions from its leading manufacturer partners. Serving the global electronic design engineer and buyer community, the global distributor's website, mouser.com, is available in multiple languages and currencies and features more than 6.8 million products from over 1,200 manufacturer brands. Mouser offers 28 support locations worldwide to provide best-in-class customer service in local language, currency and time zone. The distributor ships to over 650,000 customers in 223 countries/territories from its 93,000m², state-of-the-art distribution facilities in the Dallas, Texas, metro area. For more information, visit https://www.mouser.com.
Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.