Now at Mouser: Analog Devices' Versatile LT8361 DC-DC Converters Provide Boost/SEPIC/Inverter Configuration Options
October 22, 2018 - Mouser Electronics, Inc., the industry's leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components, is now stocking Power by Linear™ LT8361 current-mode, multi-topology DC/DC converters from Analog Devices. The versatile 2 MHz devices can be configured as boost, single-ended primary-inductor converter (SEPIC), or inverting converters, and feature a wide input voltage range of 2.8V to 60V. The converters include a 2 A, 100 V power switch, enabling them to deliver operational efficiencies up to 95 percent in automotive, industrial, telecom, and medical applications.
The Analog Devices LT8361 DC-DC converters, available from Mouser Electronics, feature a programmable frequency from 300 kHz to 2 MHz, allowing designers to avoid critical frequency bands and minimize external component sizes. The devices offer Burst Mode® operation, maintaining high efficiency at low output currents while consuming as little as 9 µA quiescent current. Spread spectrum frequency modulation delivers reduced electromagnetic interference (EMI), while a single feedback pin sets the output voltage for either positive or negative to reduce pin count.
The compact LT8361 converters are available in industrial (minus 40 to 125 degrees C) and high-temperature (minus 40 to 150 degrees C) versions, housed in a thermally enhanced, 16-lead MSOP package with four pins removed for high-voltage spacing. The feature-rich LT8361 converters also offer programmable undervoltage lockout, frequency foldback, external synchronization, programmable soft-start, and a BIAS pin for increased efficiency.
To learn more, visit www.mouser.com/adi-lt8361-converters.
With its broad product line and unsurpassed customer service, Mouser strives to empower innovation among design engineers and buyers by delivering advanced technologies. Mouser stocks the world's widest selection of the latest semiconductors and electronic components for the newest design projects. Mouser Electronics' website is continually updated and offers advanced search methods to help customers quickly locate inventory. Mouser.com also houses data sheets, supplier-specific reference designs, application notes, technical design information, and engineering tools.
About Mouser
Mouser Electronics, a Berkshire Hathaway company, is an award-winning, authorized semiconductor and electronic component distributor focused on rapid New Product Introductions from its manufacturing partners for electronic design engineers and buyers. The global distributor's website, Mouser.com, is available in multiple languages and currencies and features more than 5 million products from over 700 manufacturers. Mouser offers 23 support locations around the world to provide best-in-class customer service and ships globally to over 600,000 customers in more than 220 countries/territories from its 750,000 sq. ft. state-of-the-art facility south of Dallas, Texas. For more information, visit www.mouser.com.
About Analog Devices Inc.
Analog Devices is the leading global high-performance analog technology company dedicated to solving the toughest engineering challenges. We enable our customers to interpret the world around us by intelligently bridging the physical and digital with unmatched technologies that sense, measure, power, connect and interpret. Visit http://www.analog.com.
Trademarks
Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
(817) 804-3833
Kevin.Hess@mouser.com
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
(817) 804-7764
Kelly.DeGarmo@mouser.com