Mouser Press Room
Mouser Facebook Mouser Twitter Mouser RSS Feed Mouser YouTube Channel Mouser Google+ Mouser LinkedIn Mouser Subscription Center Mouser Blog
Mouser Press Room
New Product Announcement

 

The Future's Bright with Cree's XHP50 and XHP70 Extreme High Power LEDs Now at Mouser

The Future's Bright with Cree's XHP50 and XHP70 Extreme High Power LEDs Now at Mouser

December 22, 2014 - Mouser Electronics, Inc., the global authorized distributor with the newest semiconductors and electronic components, is now stocking the XHP50 and XHP70 XLAMP® LEDs from Cree. Setting a new standard in lighting-class LED performance with the introduction of one of the industry's first Extreme High Power (XHP) LEDs, the XHP50 and XHP70 are a new generation of Cree XLAMPs that incorporate its innovative SC5 Technology™, a platform that doubles the lumens, or light output, of a single LED. This provides lighting manufacturers with the flexibility to significantly reduce thermal, mechanical and optical costs up to 40 percent at the system level.

The Cree XHP50 and XHP70 XLAMP LEDs, available from Mouser Electronics, are the first LEDs powered by Cree's revolutionary silicon carbide SC5 Technology Platform. This platform provides twice the lumen output and improved reliability compared to previous LEDs of the same size. The XHP50 and XHP70 use fewer, more reliable LEDs to achieve the same brightness, thereby drastically reducing the size and cost of a lighting system. Cree's XHP LEDs enable engineers to design new lighting projects with less optics, a smaller printed circuit board, a smaller housing and minimized handling. Developers can also reduce heat sink size and cost, since these XHP LEDs achieve longer lifetimes even at higher operating temperatures and currents than previous LED technology - all without impacting the rated L90 lifetime of 50,000 hours (LED produces 90% of brightness after 50,000hrs).

Cree's XHP50 delivers up to 2,546 lumens at 19 watts from a 5.0 mm x 5.0 mm package, whereas the XPH70 provides up to 4,022 lumens at 32 watts from a 7.0 mm x 7.0 mm package. Both XHP LEDs offer reduced LED-to-LED color variations, are available in ANSI White and EasyWhite® 2‑step and 3‑step color temperatures ranging from 2,700 K up to 7,000 K, and offer a minimum Color Rendering Index or CRI of 70, 80 and 90. The XHP50 and XHP70 devices also offer a unique and innovative package option that allows developers to choose either 6V or 12V configurations from the same LED through the solder pad design on the circuit board.

The XLamp XHP50 and XHP70 devices from Cree are now available for purchase through Mouser Electronics. Both the XHP50 and XHP70 can help double light output and radically lower system cost, shedding the perfect amount of light intensity for a variety of next generation LED lighting applications.

To learn more about the XHP50, visit http://www.mouser.com/new/cree/cree-xhp50-xlamp-led/; for additional information on the XHP70, go to http://www.mouser.com/new/cree/cree-xhp70-xlamp-led/.

With its broad product line and unsurpassed customer service, Mouser caters to design engineers and buyers by delivering What's Next in advanced technologies. Mouser offers customers 20 global support locations and the latest, most technologically advanced components for their newest design projects. Mouser Electronics' website is updated daily and searches more than 10 million products to locate over 4 million orderable part numbers available for easy online purchase. Mouser.com also houses an industry-first interactive catalog, data sheets, supplier-specific reference designs, application notes, technical design information, and engineering tools.

About Mouser
Mouser Electronics, a subsidiary of TTI, Inc., is part of Warren Buffett's Berkshire Hathaway family of companies. Mouser is an award-winning authorized semiconductor and electronic component distributor, focused on the rapid introduction of new products and technologies to electronic design engineers and buyers. Mouser.com features more than 4 million products online from more than 500 manufacturers. Mouser publishes multiple catalogs per year providing designers with up-to-date data on the components now available for the next generation of electronic devices. Mouser ships globally to over 400,000 customers in 170 countries from its 492,000 sq. ft. state-of-the-art facility south of Dallas, Texas. For more information, visit www.mouser.com.

About Cree
Cree is a market-leading innovator of lighting-class LEDs, LED lighting, and semiconductor solutions for power applications. Cree's product families include high-brightness LEDs, lighting-class power LEDs, and power-switching devices. Cree's LED solutions are driving improvements worldwide in applications such as backlighting, electronic signs and signals. Cree is also among the world's leading manufacturers of silicon carbide-based diodes for power control and management, providing increased efficiency in a variety of applications from solar inverters to industrial motor drivers to wireless technologies.

Trademarks
Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.



Further information, contact:
Kevin Hess, Mouser Electronics
Vice President Technical Marketing
(817) 804-3833
Kevin.Hess@mouser.com
For press inquiries, contact:
Kelly DeGarmo, Mouser Electronics
Corporate Communications Manager
(817) 804-7764
Kelly.DeGarmo@mouser.com
Back to Press Room